- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
Using many of the topics (listed at the end of the thread), I've been able to turn on the PA/LNA feature on the CYBT-483056-02 module, but it seems to stop working under some conditions.
I've implemented a test command (see my previous thread which I though was solving the problem : https://community.infineon.com/t5/AIROC-Bluetooth/CYBT-483056-02-Tx-Power-setting/td-p/393817) so I can use the vendor command 0xFC14 to do a continuous TX at a given frequency.
After chipset reset and application start (configures the PA/LNA using either wiced_external_pa_lib.a or direct registers access like in the forum threads), then I can do the test command and I see the TX output on a spectrum analyzer. If I change a setting (like connectability or discoverability settings, using the wiced APIS wiced_bt_dev_set_connectability/wiced_bt_dev_set_discoverability), or if I try to connect to a remote device, then the test command will not show power any more. Also, I've observed that it was very difficult to connect to other devices, like when the PA/LNA feature is not activated.
Can you please tell us (an example would be the best) how to correctly configure the PA/LNA so that it can be used on the CYBT-483056-02 ?
Here are the two ways that I tested (these are placed in the BTM_ENABLED_EVT handler) :
status = wiced_external_pa_configure(/* ctx_pin */ WICED_P02,
/* crx_pin */ WICED_P16,
/* csd_byp_pin */ WICED_GPIO_NOT_USED,
/* epa_mode */ EPA_MODE_NORMAL);
or
(*((uint32_t *)0x338408)) = 0x48C;
(*((uint32_t *)0x338440)) = 0x47C;
(*((uint32_t *)0x338208)) = 0x600;
(*((uint32_t *)0x338240)) = 0x600;
Regards, Jerome
List of forum threads that I've looked :
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @jbruneaux ,
Attaching the power table here as well which was shared in the case management.
Thanks and regards,
Advait Kulkarni
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @jbruneaux ,
I have replied on it on the case management. Can you please check and respond there?
Thanks and regards,
Advait Kulkarni
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @advait_kulkarni ,
The distributor just forward us your answer. I'm going to check it and if I have more questions, I will go through the opened case.
One more question, why do these informations are not plublically available so that other developpers don't have to contact their distributor for these informations ? I think that the examples dedicated to the CYBT-483056-02 should already set the correct power levels and PA settings in the BSP platform initialisation so that developpers don't have to bother you with this.
Regards, Jerome
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @jbruneaux ,
Attaching the power table here as well which was shared in the case management.
Thanks and regards,
Advait Kulkarni