CYBT-343026-01 ADC Pin.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
BeKi_4844661
Level 3
Level 3
25 sign-ins 10 replies posted 10 questions asked

Dear Cypress.

Our customer want to bridge 3ch Analog audio through CYBT-343026-01.

CYBT-343026-01 ADC connect to 3ch Analog audio, is this possible?

I think CYBT-343026-01 ADC pin 2ch support, is this right?

1ch : BT Audio.

2ch: USB/SD Card

3ch: Voice.

And Is This Streaming operate at the same time Possible?

Thank you.

 

0 Likes
1 Reply
WinstonF_61
Moderator
Moderator
Moderator
250 sign-ins 100 likes received 100 sign-ins

Hi 

just to clarify, you are looking to read 3 Analog inputs on the CYBT343026 and stream mixed output over BT as a A2DP source ? 

Also if you want to use the CYBT343026 as an A2DP source the only compatible Inputs are I2S & PCM. The ADC input cannot be routed to Bluetooth as  an A2DP stream. 

Any more information would be helpful. 

 

Regards
Winston
0 Likes