AIROC™ bluetooth module flashing with USB-UART

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
SURYASUNDAR
Level 2
Level 2
First like given 50 sign-ins First solution authored

Hi,

I was trying to flash AIROC™ Bluetooth module CYBLE343072 Using FTDI USB-UART bridge while I tried to flash it showing the error 

Programming target device ...

Found serial port : COM43

Downloading FW ...
Failed to determine baud rate
Download failed

If the serial port was not detected, make sure no other program such as Client Control has the port open.

If you have issues downloading to the kit, follow the steps below:

Press and hold the 'Recover' button on the kit.
Press and hold the 'Reset' button on the kit.
Release the 'Reset' button.
After one second, release the 'Recover' button.
make[1]: *** [../mtb_shared/wiced_btsdk/dev-kit/baselib/20835B1/release-v3.3.0/COMPONENT_20835B1/make/recipe/program.mk:102: qprogram] Error 1
make: *** [../mtb_shared/core-make/release-v1.9.0/make/core/main.mk:434: secondstage_build] Error 2

Even though I tried recover reset method same error it getting. Can you suggest me to sort out this error.

0 Likes
1 Solution
advait_kulkarni
Moderator
Moderator
Moderator
25 likes received 250 sign-ins 100 solutions authored

Hi, 

Please check the following when facing this issue, that the hex file from the build folder in MTB is chosen correctly, the uart-mcu connection is shorted using jumpers and the uart port on the chip is not used or opened in any other application.

Locking this thread due to inactivity.

Thanks and regards,

Advait Kulkarni

View solution in original post

0 Likes
6 Replies
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hello @SURYASUNDAR 

Are you using a CYBLE343072 EVAL or custom board ?

If custom connection with the FTDI chip, can you please share the connection diagram and a photo of the connection?

If you already tried Recovery procedure (with reset - recovery switches) and still facing issues, then mostly it will be a hardware connection issue. 

Regards,

Anjana

0 Likes
lock attach
Attachments are accessible only for community members.

Hi
Here I am attaching the picture
HCI UART connection following-
GND - GND
VCC - VCC
RTS - CTS
CTS - RTS
RX - TX
TX-RX

0 Likes
advait_kulkarni
Moderator
Moderator
Moderator
25 likes received 250 sign-ins 100 solutions authored

Hi @SURYASUNDAR ,

We missed this issue for follow-up.

Please let us know if you are still working on this issue?

Thanks and regards,
Advait Kulkarni

0 Likes

Hi @advait_kulkarni  & @AnjanaM_61 

Myself Hemanth, 

I'm her teammate, present we are doing that project based on takeover her requirements

Now also we are facing issue on that can please suggest and sort-out the issue.

 

Thanks & Regards,

Hemanth

0 Likes
advait_kulkarni
Moderator
Moderator
Moderator
25 likes received 250 sign-ins 100 solutions authored

Hi @Hemanth1 ,

Which launch file are you choosing from MTB while downloading the code? Also can you share the PCB schematic of the  custom board so we can review it?

Thanks and regards,

Advait Kulkarni

0 Likes
advait_kulkarni
Moderator
Moderator
Moderator
25 likes received 250 sign-ins 100 solutions authored

Hi, 

Please check the following when facing this issue, that the hex file from the build folder in MTB is chosen correctly, the uart-mcu connection is shorted using jumpers and the uart port on the chip is not used or opened in any other application.

Locking this thread due to inactivity.

Thanks and regards,

Advait Kulkarni

0 Likes