Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AIROC™ Bluetooth Forum Discussions

SURYASUNDAR
Level 2
First solution authored 25 sign-ins 5 replies posted
Level 2

Hi,

I was trying to flash AIROC™ Bluetooth module CYBLE343072 Using FTDI USB-UART bridge while I tried to flash it showing the error 

Programming target device ...

Found serial port : COM43

Downloading FW ...
Failed to determine baud rate
Download failed

If the serial port was not detected, make sure no other program such as Client Control has the port open.

If you have issues downloading to the kit, follow the steps below:

Press and hold the 'Recover' button on the kit.
Press and hold the 'Reset' button on the kit.
Release the 'Reset' button.
After one second, release the 'Recover' button.
make[1]: *** [../mtb_shared/wiced_btsdk/dev-kit/baselib/20835B1/release-v3.3.0/COMPONENT_20835B1/make/recipe/program.mk:102: qprogram] Error 1
make: *** [../mtb_shared/core-make/release-v1.9.0/make/core/main.mk:434: secondstage_build] Error 2

Even though I tried recover reset method same error it getting. Can you suggest me to sort out this error.

0 Likes
2 Replies
AnjanaM_61
Moderator
Moderator First comment on KBA 5 questions asked First question asked
Moderator

Hello @SURYASUNDAR 

Are you using a CYBLE343072 EVAL or custom board ?

If custom connection with the FTDI chip, can you please share the connection diagram and a photo of the connection?

If you already tried Recovery procedure (with reset - recovery switches) and still facing issues, then mostly it will be a hardware connection issue. 

Regards,

Anjana

0 Likes
SURYASUNDAR
Level 2
First solution authored 25 sign-ins 5 replies posted
Level 2

Hi
Here I am attaching the picture
HCI UART connection following-
GND - GND
VCC - VCC
RTS - CTS
CTS - RTS
RX - TX
TX-RX

0 Likes