3D Hall (Magnetic sensor) Forum Discussions
初始化过程过中,有一步是读取0-9的读寄存器,并存储7,8,9寄存器用于配置使用。
问题一,我发送复位信号后,进行读取0-9的读寄存器,如寄存器0H,有时01H,有时为00H,有时为FFH。我看到数据手册Reset后应该为00H。请问此时寄存器0H是可以不予理会,还是要重复进行Reset,直到读取的值为00h。其他情况例如寄存器0,1,2,3,6。
问题二:还是不理会从取0-9的读寄存器的值,只要从机有给主机应答信号就行。
Show Less
初始化过程过中,有一步是读取0-9的读寄存器,并存储7,8,9寄存器用于配置使用。
问题一,我发送复位信号后,进行读取0-9的读寄存器,如寄存器0H,有时01H,有时为00H,有时为FFH。我看到数据手册Reset后应该为00H。请问此时寄存器0H是可以不予理会,还是要重复进行Reset,直到读取的值为00h。其他情况例如寄存器0,1,2,3,6。
问题二:还是不理会从取0-9的读寄存器的值,只要从机有给主机应答信号就行。
Show Less
Hi,
I'm working with the mentioned generic library software for TLx493d, downloaded from the infineon homepage (see picture in attachment)
There I´ve found an error in the AW2B6 sub-category:
In the init function: TLE493D_AW2B6_init (file: TLE_AW2B6.c)
The configurable bits of the address are added into the register and afterwards when the other config bits of the register are set, an | is missing in line 228 (should be |= instead of =), which causes the set address-bits to be overwritten with zeros again and sensors are always set to A0 address independent from which address was chosen before or which version sensor(A0-A4) was used.
Please forward this to the right person to have it fixed, as it was a bit tricky to find and prevend other people from having those issues.
Thanks.
BR
Alexander Frank
how to program TLV493D-A1B6 sensor using stm32 to get X,Y,Z and Temperature values.
It took a while to find the correct I2C sensor address of 0x22 but now I can finally talk to the sensor.
However, when taking readings from the senor it is sending a response of 0xFF for all registers.
I have tried using 2-byte read (supposed default) as well as 1-byte read just in case.
I really need to have this working as soon as possible so any help would be greatly appreciated!
Thank you. Show Less
TLV493D-A1B6 使用/INT的中断读取数,器件是否一直读取数据,能否停止下来,进行模式切换。
Hello Yashraj/ Moderator,
I am sorry for late information. Replies to previous thread which I have created has landed in my mailbox in Junk folder, so I couldn't reply timely.
We are using TLV493D-A1B6 for detecting the tampering of E-Meter. Our SoC runs Linux, so we are looking for linux device driver for the sensor. First search in google didn't show any available device drivers in Linux kernel. Please guide me if there are any already available or compatible drivers available.
Best Regards,
Abhishek
Hi
To refer to the data sheet, TLE4988CXTNM28 is a programmable chip. How can I find more information about it?
Dear Team,
What is the right fit suggestion for Rollover sensor from Infineon for 2-Wheeler EV Application