- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hello everybody,
I have some problems to communicate with a 2D hall sensor from Infineon via I2C.
First some background information:
CY8CKIT-42 PSoC 4 Pioneer Kit
PSoC Creator 4.4
TLE493D-A2B6 (https://www.infineon.com/dgdl/Infineon-TLE493D-W2B6-UM-v01_01-UserManual-v01_11-EN.pdf?fileId=5546d4...
I wrote myself two functions which allow me to read or write a register.
The TLE493D has a 2-byte read command and a 1-byte read command. So I try to write the register first and change it to 1-byte read command mode.
When I try to write a register, it works, but when I try to read a register, I always get a NACK after I send the register address of the sensor. I don't know what the problem is.
I tried the read function with a MPU6050 sensor and it worked. I could read the register.
Why can't I read the registers properly?
I have added some pics and the project in the attachment.
Best Regards and Thank You
Michael
Solved! Go to Solution.
- Labels:
-
PSoC 4 MCU

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,
I think you just need to change your read routine so that it uses the I2C_1_I2C_MODE_COMPLETE_XFER flag, they are two separate processes that have to be completed acknowledged separately,
when using this flag I2C_1_I2C_MODE_NO_STOP you would not use the API Write/Read Buffer but work with Bytes instead
uint8 tle493d_ReadReg(uint8 Reg)
{
uint8 Write_Buf[1] = {0};
Write_Buf[0] = Reg;
uint8 Read_Buf[1] = {0};
I2C_1_I2CMasterWriteBuf(TLE493_ADDRESS,(uint8 *)Write_Buf,1,I2C_1_I2C_MODE_COMPLETE_XFER );
while((I2C_1_I2CMasterStatus() & I2C_1_I2C_MSTAT_WR_CMPLT)== 0){}
I2C_1_I2CMasterReadBuf(TLE493_ADDRESS, (uint8 *)Read_Buf,1,I2C_1_I2C_MODE_COMPLETE_XFER );
while((I2C_1_I2CMasterStatus() & I2C_1_I2C_MSTAT_RD_CMPLT) == 0){}
return Read_Buf[0];
}
hope it helps

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,
I think you just need to change your read routine so that it uses the I2C_1_I2C_MODE_COMPLETE_XFER flag, they are two separate processes that have to be completed acknowledged separately,
when using this flag I2C_1_I2C_MODE_NO_STOP you would not use the API Write/Read Buffer but work with Bytes instead
uint8 tle493d_ReadReg(uint8 Reg)
{
uint8 Write_Buf[1] = {0};
Write_Buf[0] = Reg;
uint8 Read_Buf[1] = {0};
I2C_1_I2CMasterWriteBuf(TLE493_ADDRESS,(uint8 *)Write_Buf,1,I2C_1_I2C_MODE_COMPLETE_XFER );
while((I2C_1_I2CMasterStatus() & I2C_1_I2C_MSTAT_WR_CMPLT)== 0){}
I2C_1_I2CMasterReadBuf(TLE493_ADDRESS, (uint8 *)Read_Buf,1,I2C_1_I2C_MODE_COMPLETE_XFER );
while((I2C_1_I2CMasterStatus() & I2C_1_I2C_MSTAT_RD_CMPLT) == 0){}
return Read_Buf[0];
}
hope it helps
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hello jepaz, thx for the advice. I wanted to reply yesterday, but the forum was locked. I've tried it out, but it was the same. I have found another error and I have set the wrong bits in the register, because in the example I am follwing the values were in DEC and I have written them in HEX. So maybe it don't work, because I haven't change the config and mode register.
But I've written a new function. The function reads all 23 registers and stores the content in an array. I have stored only the relvant ones for me in variables. I doesn't run perfectly, but at least I get the values. (https://github.com/Infineon/TLE493D-3DMagnetic-Sensor/issues/13)
uint8* tle493d_read()
{
static uint8 Read_Buf[23] = {0};
I2C_1_I2CMasterReadBuf(TLE493_ADDRESS,(uint8 *)Read_Buf,23,I2C_1_I2C_MODE_REPEAT_START);
while((I2C_1_I2CMasterStatus() & I2C_1_I2C_MSTAT_RD_CMPLT) == 0){}
return Read_Buf;
}
I wanted add a UART interface, but somehow I mess up the source code or the project. Now I get no values and I have to clean up my code.
The sensor seems to be okay, because with an arduino nano I get plaubisble values.
I will be in touch if I get stuck and need some help
Best Regards
Michael