公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
qq963598371
Level 1
Level 1
First question asked First reply posted
芯片的介绍首页的供电等级是5.5V~40V。芯片手册中给出额定工作电压是8~17V,工作时扩展电源电压是5.5~40V。这个芯片,内部集成电荷泵,电荷泵输出电压应该高于电源电压8V以上,不然不能正常工作,实际我给24V电源电压,电荷泵输出却只有29V,芯片不能工作。我给19V电源电压,倒是可以正常工作。电荷泵电路只有3个电容,所以我怀疑时电源电压实际不能到40V,芯片介绍页给的参数是有问题的。现在我想在24V系统中使用这颗芯片,发现要实现19V电源输入,还有一定技术问题。所以来这里寻求一下是否有24V系统中使用这颗芯片的可能。
0 点赞
3 回复数
Anonymous
不适用
最好找一下英飞凌的FAE
0 点赞
qq963598371_
Level 1
Level 1
First question asked First reply posted
可能需要满足Vbat大于Vsup的要求。我现在是连一起的。但是很多单片机手册也要求VDD和VDDA大小关系,连一起也没问题。
0 点赞
SIX_66
Level 6
Level 6
First comment on blog 500 replies posted 250 replies posted
学习学习
0 点赞