公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

【LED】TLD2131_3EP/TLD2331_3EP 可以将OUT_SET引脚连接到2个IN_SET引脚吗?

【LED】TLD2131_3EP/TLD2331_3EP 可以将OUT_SET引脚连接到2个IN_SET引脚吗?

minwoo
Level 2
Level 2
First solution authored 25 replies posted 10 replies posted

在LITIXTM Basic+系列中的OUT_SET引脚,反映了由外部电阻RSET定义的IN_SET电流,可以用来定义额外同组器件的IN_SET电流。OUT_SET引脚在应用层中定义了额外器件的输出电流而无需额外外部器件。

将器件1的OUTSET引脚连接到器件2的两个INSET引脚是不可能的,如下图所示。

QQ截图20230227152143.png

2个VIN_SET(ref)可能略有不同,这可能会导致电流不匹配。更具体地说,具有较低阻抗的INSETx引脚将取代另一个INSETx'引脚。在这种情况下,如果IN_SET2的阻抗低于IN_SET3的阻抗,则表明只有OUT2上的LED处于可控状态(LED ON连接到OUT2,LED OFF连接到OUT3)。

OUT_SET引脚只能连接到一个IN_SET引脚,如下面配置所示:

QQ截图20230227152203.png

 这样,TLD2131-3EP的OUT_SET引脚连接到TLD2331-3EP的IN_SET2引脚。

IN_SET3引脚连接到电阻RSET3,两个输出通道均处于可控状态。

由于每个器件的IN_SET引脚上仅使用了1个电阻,而不是2个或更多,所以减少了物料清单(BOM)。


0 点赞
408 次查看