Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Alexa Skills Demo on PSoC 6 WiFi BT Prototyping kit

lock attach
Attachments are accessible only for community members.

Alexa Skills Demo on PSoC 6 WiFi BT Prototyping kit

SriJ_56
Employee
Employee
First question asked 5 sign-ins First like received

Alexa Skills Demo on PSoC 6 Wi-Fi BT Prototyping Kit

1. Objective

The objective of this blog is to explain how to use Alexa Skills to control ‘things’ using PSoC 6 Wi-Fi BT Prototyping kit. We will control the speed of a fan on PSoC thermal management expansion board by instructing an Alexa device.

 

2. Requirements

Hardware:

      1. CY8CPROTO-062-4343W PSoC 6 Wi-Fi BT Prototyping kit
      2. CY8CKIT-036 PSoC thermal management expansion board kit
      3. Amazon Echo device (use Alexa simulator in the Alexa Skill Developer console if echo device is not available)

Software:

      1. Amazon developer account to use Alexa Skill developer console
      2. AWS account to use
        1. Compute service - Lambda
        2. Security, Identity, & Compliance service – IAM
        3. Internet of Things service – IoT core
      3. Mbed CLI to run subscriber application on PSoC 6 using Mbed OS ecosystem
      4. Serial terminal (Eg. Tera term) to view output and debug messages.

3.   Summary

Figure 1. Data flow from Amazon Echo to the fan

pastedImage_40.png

Amazon Echo is tuned to our use case of controlling the speed of a fan by building a custom skill using Alexa Skills Kit.

The developed custom skill is hosted on AWS Lambda service. Lambda function is triggered from Alexa Skills and the function is coded to publish messages to a topic in AWS IoT based on the input from the developed custom Alexa skill.

The physical device (PSoC6 + 4343W) subscribes to this topic in AWS IoT and generates appropriate PWM signal to control the speed of the fan. In this project, we will operate the fan at three different speeds namely low speed, mid speed and high speed.

 

Low speed

20% duty cycle (0 to 20% duty cycle will operate the fan in the kit at   its minimum speed).

Mid speed

50% duty cycle

High Speed 100% duty cycle
 

However, in case of general instructions to Turn On/Off or increase/decrease of the speed, following will be the behavior.The user is expected to control the fan by asking Alexa to set or run at one of these speeds.

However, in case of general instructions to Turn On/Off or increase/decrease of the speed, following will be the behavior.

 

  Turn On

  Fan will run at mid speed
  Turn Off   Fan will run at low speed
  Increase the speed   Fan will run at high speed
  Decrease the speed   Fan will run at low speed
          

4. Setting up the project

 

     4.1.  Building Custom Skill

    1. Login Amazon developer account and navigate to Alexa developer console.
    2. Choose Create skill.
    3. Enter name of the skill and leave the rest at default as shown in Figure 2.

               (Ensure default language is English (US).

               Default settings allows us to create a custom skill and use our own AWS lambda endpoint)

 

Figure 2. Alexa Custom Skill Creation

ASK create skill.png

            4.  Choose template as Start from scratch.

            5.  Start building the custom skill by

                     a. Entering an invocation name – ‘fan controller’ is used in this project. This name is required for launching our custom skill.

                     b. Adding custom intents and utterances –

                         We will add an intent for each of the three speeds that we intend our fan to operate at,

                         namely LOW_SPEED, MID_SPEED and HIGH_SPEED.

                         Add all those phrases the user might utter to achieve the intent’s functionality as its sample utterances.

                         Either create the intents from the GUI in the developer console or use the provided JSON file (intents.json) and copy paste

                         the contents in the JSON editor tab.

                     c. ‘Save model’ followed by ‘Build Model’ and ensure error free build.

                     d. Test your model by using ‘Evaluate model’. Entering a sample utterance should invoke the correct intent.

                     e. Go to Endpoints -> Choose AWS Lambda ARN. Copy the skill Id. This is required in the AWS Lambda services.

                         We will return to the Alexa developer console and add the ARN of the lambda function we create in Section 4.2.

     Refer to Alexa documentation for developing custom skill for more detailed explanation of creating custom skills.

4.2.  Set up AWS IoT core

AWS IoT core requires the following to be set up

1.       Things - Things refer to a representation of the physical device.

2.       Certificates - Certificates should be created to ensure secure communication between AWS and the device.

3.       Policies - you must create and attach an AWS IoT policy that will determine what AWS IoT operations the thing may perform.

 

Follow the instructions in the amazon documentation to create things, certificates, policies and attach the policies to certificates.

Ensure to have same region selected for AWS lambda and AWS IoT core.

Regions can be selected at the top right corner in both the consoles. N.Virginia (US EAST region was selected in this project).

4.3.  Creating Lambda function

    1. From AWS home page, open lambda services by navigating through Services -> Compute -> Lambda
    2. Choose to create function -> Author from scratch
      1. Enter a function name.
      2. Choose Node.js 12.x
      3. Leave ‘choose/create execution role’ at default (i.e create a new role with basic lambda permissions).
    3. Once the function is created, add a trigger from Alexa Skills Kit. Enable skill id verification and paste the copied skill id from the Alexa skills endpoint section.
    4. Scroll down to the code function area and copy the code provided as index.js to the console.

                Leave the rest at default.

            5. Modify the lambda function to interact with the ‘thing’ related data in AWS IoT.

                    a. Insert Endpoint of your ‘thing’ from the IoT AWS core.

                        Navigate to Things -> Interact and choose the REST API endpoint in the IoT AWS core.

Figure 3. Thing Endpoint in lambda function

pastedImage_68.png

                    b. Change the ‘thing’ name in the lambda function per the thing created in AWS IoT as shown below.

Figure 4. Thing name in lambda function

pastedImage_148.png

 

          6. Copy the ARN of your lambda function. Add this to the default region of AWS Lambda ARN in the Alexa Skills Endpoint.

              This is required for invoking this lambda function when the user interacts with ASK.

4.4.  IAM set up

We need to create an IAM policy that provides the minimum required permissions for Alexa Skills to invoke an AWS Lambda function.

      1. Open IAM from AWS home by navigating to Services à IAM (under Security, Identity, & Compliance)
      2. Select Roles and click on the role corresponding to the lambda function created as shown in figure below.

Figure 5. IAM Roles

pastedImage_4.png

(*Exact screenshots may differ)

                    3. Click the policy name under permissions tab. Choose Edit policy.

                        Go to JSON tab and copy the content from the attached policy (IAM policy.json).

                        Click on review policy -> save policy.

4.5.  Creating Subscriber Application

                    1.    Install Mbed CLI and Mbed Serial Port driver. Refer to Mbed documentation for more details.

                    2.   Use the PSoC 6 +4343W Prototyping kit in DAPLink mode. Hold SW3 switch for >2 seconds and release.

                          The status LED (LED2) should ramp up an amber light at 2Hz.

                          If you face any issues in entering DAPLink, ensure the kit has latest KitProg3 firmware.

                          Refer to KitProg3 user guide for more details.

                    3. Clone the Code example ‘mbed-os-example-aws-iot-client’.

                         This example connects to a WiFi network and can subscribe to messages from the AWS cloud using the

                         Mbed OS ecosystem from github.

                    4. Enter the subscriber directory and follow the Instructions below to build AWS IoT subscriber code example.

        a.   Change to the application folder (subscriber)

        b.    Prepare the cloned working directory for mbed by entering the following command in command prompt.

   mbed config root .

        c.     Pull the necessary libraries and its dependencies.

                  This will pull mbed-os, AWS_Iot_Client library and its internal 3rd party dependencies

     mbed deploy

        d.     Configure the SSID and password of the desired network in the mbed_app.json file.

                  Replace the word ‘SSID’ with name of the network and similarly for the password.

        e.    Configure the AWS parameters such as Thing name, certificates, private key per the user's AWS account.

            Use the attached sample_aws_config.h for reference.

        f.      Also, configure the AWS topic to be subscribed to receive the messages.

              The lambda code provided in the example updates to shadow of the ‘thing’.

              We will subscribe to the ‘shadow delta’ to receive the messages.

              Refer to Amazon Documentation on shadows for more details.

        g.   We receive messages from AWS thing shadow in JSON format.

              We will use a JSON library to extract the desired state from the JSON formatted message.

        Download the zip JSON parser and extract the contents.

       Create a folder, say mbed-json-parser inside the subscriber folder and place the extracted .cpp and .h files in that folder.

        h.    Replace the subscriber.cpp file in the subscriber folder with the subscriber.cpp file provided.

        i.     Modify the default AWS packet size to high value.

             This is needed to receive the entire message from the shadow and then extract the required state in our subscriber application.

                This macro is available in

                …\mbed-os-example-aws-iot-client-master\subscriber\aws-iot\aws_client.h file.

                Modify AWS_MAX_PACKET_SIZE to 1000 as shown.

                By default, it is set to 100.

Figure 6. Increasing AWS Packet Size

Capture.PNG

                             j. Build the project using mbed compile --target CY8CPROTO_062_4343W --toolchain GCC_ARM

                             k. Hex file generated can be found in

                                 …\mbed-os-example-aws-iot-client\subscriber\BUILD\CY8CPROTO_062_4343W\GCC_ARM.

        Program the hex file using Cypress Programmer or drag and drop the hex file to the DAPLINK drive.

        Alternately, use mbed compile --target CY8CPROTO_062_4343W --toolchain GCC_ARM -f to compile and program.

5. Testing the project

5.1.  Hardware connections:

CY8CPROTO-062-4343W kit is connected to CY8CKIT-036 as shown.

DGND of both the kits are connected. PWM signal for fan 1(PWM1) is connected to P8.7 in this example.

 

Figure 7. Hardware set up

pastedImage_84.png

5.2.  Test Execution

    1. Set up serial Terminal. Connect to the Mbed serial port with a baud rate of 115200.
    2. Speak out the commands to the Echo device/Alexa simulator. Alternatively, you can type the utterances in the simulator. Alexa simulator is available in the ‘test’ tab of your developed custom skill.

   Ensure to select the same language as in Amazon developer account is selected in Alexa Mobile App while setting up the  Amazon Echo device.

   Refer to the Amazon documentation for more details on testing the custom the skill.

   Eg utterances:

        1. Alexa, ask fan controller to set high speed
        2. Alexa, Set low speed from fan controller
        3. Alexa, ask fan controller to run the fan at medium speed

               In these examples, fan controller is the invocation name.

               This must be used in the sentence to launch the custom skill along with connection words such as ask,tell, from etc.

               Refer to Alexa Documentation for more details on how to invoke custom skills.

5.3.  Expected Outputs:

    1. Fan should run at the desired speed.

            2. Echo device/simulator should respond back with the speed at which the fan is running.

                Note: If expected behavior is not observed when using the Echo device,

                please check if Alexa was able to process your speech correctly.

                In the Alexa App, Navigate to Settings -> Alexa Privacy -> Review Voice History to check your interactions with Alexa.

            3. Alexa Simulator Output

                Enter test tab and type the utterance. Alexa skills responds with the output as shown in figure below.

Figure 8. Alexa test (Simulator)

pastedImage_85.png

 

          4. AWS IoT Output

              Enter the activity tab and observe the shadow state being updated as shown.

Figure 9. AWS IoT shadow

pastedImage_86.png

        5. Serial Terminal Output

Figure 10. Tera Term Output

pastedImage_0.png

 

Thank you! Enjoy controlling physical devices using PSoC 6 + 4343W through Alexa!

 
Attachments
2334 Views
Comments
NaAm_1281831
Level 2
Level 2
First comment on KBA 10 replies posted 10 sign-ins

Hello,

  I would like to modify this project to control LED ON and OFF , I can use this tutorial as reference to create Alexa skill for LED on and OFF, but I am not really sure how to modify/develop the LAMBDA function even though i am familiar with NodeJS programming.

Please shar me any useful links or modified Lambda function.

NaAm_1281831
Level 2
Level 2
First comment on KBA 10 replies posted 10 sign-ins

Never mind, I followed your instructions and modified your Lambda code to turn on/off the led, I am attaching my LED ON/OFF intents JSON file and LAMBDA functions here incase somebody wants to use it. https://www.dropbox.com/s/zduvonc9eoduxdj/LED_Attachments.zip?dl=0