WICED application framework and manufacturing image in CYW943907AEVAL1F
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
This blog discusses the different binaries that are downloaded in CYW943907AEVAL1F EVK when the board is programmed using WICED SDK. This blog also addresses the procedure of creating a single binary suitable for manufacturing. Please note that the manufacturing image procedure is explained for ota2 compatible image. The same method can be followed to create a similar image for generic case(non OTA2).
WICED FRAMEWORK:
The different binaries needed for programming a CYW943907AEVAL1F EVK are
1. Bootloader
2. DCT
3. APPS LUT
4. FILESYSTEM
5. APPLICATION(There can be multiple applications APP0, APP1, APP2)
During a normal build process, the files which are downloaded can be viewed by including VERBOSE=1 in the make target. The downloaded files from the build log are shown below:
1. DCT
Downloading DCT ... build/<snip_name>-CYW943907AEVAL1F/DCT.bin @ SFLASH_DCT_LOC=0x00008000
2. The Bootloader file is:
build/waf.bootloader-NoOS-NoNS-CYW943907AEVAL1F-P103-SoC.43909/binary/waf.bootloader-NoOS-NoNS-CYW943907AEVAL1F-P103-SoC.43909.trx.bin
3. Filesystem is created with
./tools/common/Win32/mk_wicedfs32 build/<snip_name>-CYW943907AEVAL1F/filesystem.bin build/<snip_name>-CYW943907AEVAL1F/resources/Staging/
and downloaded
Downloading resources filesystem ... build/<snip_name>-CYW943907AEVAL1F/filesystem.bin at sector 17 size <filesystem_size>...
4. Downloading Application
Downloading APP0 build/<snip_name>-CYW943907AEVAL1F/binary/<snip_name>-CYW943907AEVAL1F.stripped.elf @ sector <filesystem_start_address + filesystem_size> address xxx size <filesystem_size>...
5. APPS LUT
Downloading apps lookup table in wiced_apps.mk ... build/<snip_name>-CYW943907AEVAL1F/APPS.bin @ 0x00010000 size
How are the addresses determined for programming the binaries/files?
>> The memory map is defined in <WICED- SDK>\43xxx_Wi-Fi\platforms\CYW943907AEVAL1F\normal_image_defines.mk
The starting address of filesytem is given as:
In /43xxx_Wi-Fi/platforms/CYW943907AEVAL1F/normal_image_defines.mk,
NORMAL_IMAGE_APPS_AREA_BASE := 0x00011000 i.e, 69632 d
In /43xxx_Wi-Fi/WICED/platform/MCU/BCM4390x/BCM94390x_common.mk
APPS_START_SECTOR := $(shell $(PERL) $(SECTOR_NUMBER_SCRIPT) $(NORMAL_IMAGE_APPS_AREA_BASE) $(SECTOR_SIZE))
Hence APPS_START_SECTOR=69632/4096 = 17
The starting address of application stripped.elf is obtained by adding the filesystem size to APPS_START_SECTOR.
Kindly check the BUILD_APPS_RULES in 43xxx_Wi-Fi/tools/makefiles/wiced_apps.mk for understanding the computation of starting sectors.
MANUFACTURING IMAGE:
The manufacturing image is a single image suitable for download during manufacturing.
WICED has implemmenttaion for creating manufacturing image suitable for OTA2. It follows the memory map defined in 43xxx_Wi-Fi\platforms\CYW943907AEVAL1F\ota2_image_defines.mk
The image is created using "ota2_manuf_image" in the make target.
How is the manufacturing image created and which files are included in it?
>> Please look for ota2_manuf_image target in 43xxx_Wi-Fi\tools\makefiles\wiced_apps.mk
First a manufacturing config file is created.
$(QUIET)$(call WRITE_FILE_CREATE, $(OTA2_IMAGE_MANUFACTURING_CONFIG_FILE) ,$(OTA2_IMAGE_BOOTLOADER_START) build/$(BOOTLOADER_TARGET)/binary/$(BOOTLOADER_TARGET).trx.bin)
The config file is than appended with information of other required binaries. One such example is:
$(QUIET)$(call WRITE_FILE_APPEND, $(OTA2_IMAGE_MANUFACTURING_CONFIG_FILE) ,$(OTA2_IMAGE_FACTORY_RESET_AREA_BASE) $(OTA2_IMAGE_FACTORY_RESET_BIN_FILE))
The config file is then passed to a tool which creates the image. The image is filled with 0xFF for unused parts of the FLASH
$(shell $(PERL) $(CREATE_FLASH_IMAGE_TOOL) $(call CONV_SLASHES,$(OTA2_IMAGE_MANUFACTURING_CONFIG_FILE)) $(call CONV_SLASHES,$(OTA2_IMAGE_MANUFACTURING_BIN_FILE)))
The $(CREATE_FLASH_IMAGE_TOOL) is located @43xxx_Wi-Fi\tools\common\<OS>\mk_wiced_ota2_image32.exe