List of Applications supported in WICED Studio 5.0 (or later) for CYW943907AEVAL1F EVK
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
The following table lists all applications that are supported within WICED Studio 5.0(or later) on the CYW943907AEVAL1F EVK .
Please refer to the CYW943907AEVAL1F EVK User Guide when compiling, downloading and debugging applications with this platform.
Sl.no | Location inside WICED Studio (. signifies next level path) | Description |
---|---|---|
1. | snip.gpio | Demonstrates how to use WICED GPIO API to toggle LEDs and read button states |
2. | snip.scan | This application snippet regularly scans (by default once in every 5 secs) for nearby Wi-Fi access points and prints information about the same. |
3. | snip.apsta | Demonstrates Wi-Fi client mode (to send a regular ICMP ping to an AP) and |
4. | snip.crypto |
demonstrates how to use crypto functions available in the WICED crypto library |
5. | snip.custom_ie |
This application snippet demonstrates how to add and remove custom (Information Elements) IEs in AP Beacons, using Wi-Fi softAP interface. |
6. | snip.dct_read_write |
This application demonstrates how to use the WICED DCT (Device configuration Table) API to access the WICED DCT. |
7. | snip.ap_clients_rssi |
This application snippet demonstrates how to retrieve a list of Wi-Fi clients associated to the WICED softAP and obtain the RSSI (signal strength) for each client. |
8. | snip.coap_app |
This application snippet demonstrates how to react to COAP packet from network client and activate the services exported by Coap. |
9. | snip.config_mode |
This application demonstrates how to use WICED Configuration Mode to automatically configure application parameters and Wi-Fi settings via a softAP and webserver |
10. | snip.wps_registrar |
This application snippet demonstrates how to use the WPS Registrar on an existing softAP interface |
11. | snip.http_server_sent_events | This application snippet demonstrates how to send events from a HTTP server back to its clients. |
12. | snip.https_client |
This application snippet demonstrates how to use the WICED DNS (Domain Name Service) & HTTPS API |
13. | snip.https_server |
This app connects to a Wi-Fi network as a STA (client), then starts a secure web-server and waits for requests. It also starts a non-secure web-server which provides a redirect that redirects any non-secure requests to the secure webpages. |
14. | snip.led_example | This application demonstrates how to use daemons/led_service to turn LEDs on and off, display patterns. |
15. | snip.link_status |
This application demonstrates how to asynchronously handle changes in the Wi-Fi link connection status. |
16. | snip.stdio | This application demonstrates how to use the UART for STDIO operations. |
17. | snip.tcp_client |
This application snippet demonstrates how to connect to a Wi-Fi network and communicate with a TCP server |
18. | snip.tcp_server |
This application snippet demonstrates how to used the WICED TCP API to implement a TCP server |
19. | snip.thread_monitor |
This application demonstrates how to use the WICED System Monitor API to monitor the operation of the application thread. |
20. | snip.uart |
This application demonstrates how to use the generic WICED UART API to send and receive characters on the UART. |
21. | snip.websocket_client | This application snippet demonstrates how to use a simple Websocket Client protocol. |
22. | snip.wps_enrollee | This application snippet demonstrates how to use the WPS Enrollee |
23. | test.console | This application demonstratest test console which can be used for a variety of commands including iperf, ping, etc. |
24. | demo.appliance |
This application demonstrates how a simple web page can be used to send information to a UART when a button on the webpage is clicked. |
snip.wps_registrar