Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

SN8000 WiFi Module with STM Discovery Board

lock attach
Attachments are accessible only for community members.

SN8000 WiFi Module with STM Discovery Board

SeyhanA_31
Employee
Employee
250 replies posted 100 replies posted 50 replies posted

Here is an example of interfacing the BCM43362 based SN8000 WiFi module (from Murata) with STM32F4-Discovery board (with STM32F407 MCU).

 

The schematic below illustrates the connections required to connect the SN8000 to the STM32F4-Discovery board. Since the SN8000 comes as a module to connect to a PCB, a carrier board is needed to connect the module to the STM32F4-Discovery board.

ScreenHunter_95 Jan. 02 16.15.jpg

pastedImage_1.png

 

If you have the SN8000 module mounted on a SDIO carrier board, which comes with the SN800 evaluation board, the following connection schema can be used to connect the module to the STM32F4-Discovery board.

ScreenHunter_97 Jan. 02 16.19.jpg

pastedImage_4.png

 

For terminal interface between the STM32F4-Discovery board and host PC the following serial (RS232) connection is needed.

pastedImage_6.png

To connect a JTAG debugger (Olimex_ARM-USB-TINY-H) to the STM32F4-Discovery board follow the below connection.

pastedImage_0.png

For more information please take a look at this link: Interfacing STM32Fx-Discovery with WICED using JTAG Debugger

 

After setting up the hardware connections WICED SDK-3.x should be updated to run WICED applications on STM32F4-Discovery board with SN8000 WiFi module. Unzip the attached file with the following expected updates.

 

The STM32F407 directory goes to .../WICED/platform/MCU/STM32F4xx/GCC directory of the WICED SDK.

pastedImage_7.png

 

The STDiscovery407_BCM43362 platform files goes to .../platforms directory of the WICED SDK.

ScreenHunter_104 Jan. 02 22.35.jpg

 

To build and run application using WICED SDK following Make Target could be used;

     <Application>-STDiscovery407_BCM43362 JTAG=Olimex_ARM-USB-TINY-H download run

 

To build and run a sample scan app use the following Make Target:

     snip.scan-STDiscovery407_BCM43362-debug JTAG=Olimex_ARM-USB-TINY-H download run

Attachments
2120 Views