Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

How to bring a WICED SDK into Eclipse

How to bring a WICED SDK into Eclipse

SeyhanA_31
Employee
Employee
250 replies posted 100 replies posted 50 replies posted

Copy the WicedSDK source where you like. For this example the WicedSDK is copied into the C:\MyWicedSDKs2.4.1 directory.

 

1. Create an eclipse workspace at C:\MyWicedSDKs2.4.1.

Select "File" -> "Switch Workspace" -> "Other..."

pastedImage_3.png

 

2. Select the directory where the WicedSDK is located.

pastedImage_10.png

 

3.Create a new “C Project” by selecting “File” -> “New” -> “C Project”.

Project type: select “Empty Project” under “Makefile project”.

Project Name: enter MyWicedSDK then select “Finish”.

pastedImage_3.png

4. Select MyWicedSDK on “Project Explorer” tab then select “Project” -> “Properties”.

pastedImage_4.png

5. Select “C/C++ Build” then deselect “Use default build command” and update “Build command” to “${workspace_loc:/MyWicedSDK}/make.exe” for Windows.

Then select “OK”.

pastedImage_8.png

 

6. Select MyWicedSDK on “Project Explorer” tab then select “Project” -> “Make Target” -> “Create…”

pastedImage_20.png

 

For “Target name” type “clean” then select “OK”.

pastedImage_23.png

 

In the "Make Target" tab, the folder icon pastedImage_27.png should be selected (if it is not by default) to show the “Clean” target command under “Make Target” tab.

 

7. Double click on pastedImage_31.png icon to run “make clean” command for MyWicedSDK project.

pastedImage_32.png

 

8. To verify everything is working, let's use step 6 from above to create a sample scan application target:

For “Target name:” instead of "clean" enter “snip.scan-BCM943362WCD4 download run”.

Connect the appropriate hardware BCM943362WCD4 to the host PC.

Double click on “snip.scan-BCM943362WCD4 download run” to build download and run the scan test application.

pastedImage_36.png

1496 Views