Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Welcome to the Infineon Developer Community

  • 71438 Discussions

  • 43019 Members

  • 41855 Solutions

filter icon

Recent discussions

Sort by:
Filter by forum
Ahmedms
USB superspeed peripherals
Hi, I used the cyfxgpiftousb example to read data from the AD7381-4 ADC (Project attached). <<First, the intention is to stream data continuously from... Show More
Nathen
AURIX™
hey guys I am trying to implement the latest DSPLIB V9.2 using Aurix development studio,after following the guidence “AP32528_Getting_started_with_Aur... Show More
Communication
PSoC™ 6
  Hello friends!I am doing a circuit project using DHT11 sensor and soil moisture sensor, reading sensor using PSoC 063 BLE, I use Protues software to... Show More
kilohercas
PSoC™ 5, 3 & 1
Hello,We had encoders failed from our supplier, and they are using CY8C5888NI-LP210 microcontroller. What is failed is quadrature outputs on P12[4], P... Show More
zhuxiaozhu
MOSFET (Si/SiC)
各位好,最近我在做一版飞跨电容型三电平Buck电路,在做单电压闭环(飞跨电容电压平衡暂未控制)时出现了在输入达到20V以上后,输出电压开始下降的问题,已知信息如下。 1.采样选用隔离放大器+普通运放调理的电路,用稳定直流电压测试没有问题。 2.采用我的电路板,在开环状态下以不同的占空比输出相同电压(... Show More
qwertyqwq35
Motor Control ICs
Hi all, Since my last new pcbs arrived im struggiling to drive my motor smooth. And here what are my problems about running my motor. First of all , t... Show More
shaun_pye
AURIX™
Hello, How can the effectiveness of the external capacitor be evaluated for EDSADC? There is no information about the internal switched capacitor or o... Show More
BBasheer
PSoC™ 6
Hi Surprisingly, CY8C6245AZI-S3D72 PG-TQFP-100 is unavailable in PSOC Creator / ModusToolbox / Eclipse IDE.   Our project halted as this device not av... Show More
Sandy_d
AURIX™
Hi there, In my software development, I have a use case where the external variable is defined in one partition and accessed and cleared in other part... Show More
Akhilesh
AURIX™
Hello Team, I was trying to build an application that uses multiple cores. I am able to generate the elf file as well. When I try to run the elf, only... Show More