Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Welcome to the Infineon Developer Community

  • 73898 Discussions

  • 46649 Members

  • 44120 Solutions

filter icon

Recent discussions

Sort by:
Filter by forum
CHenze
MOSFET (Si/SiC)
Is there any special consideration when using a pair of SiC or GaN FETs (compared to regular silicon FETs) in a common source configuration  to create... Show More
mngr05
Motor Control ICs
Hello, I am having a strange problem, I cannot push the motor over a certain speed.I have a 7200rpm motor, but I am able to make it spin only up to ne... Show More
drudolf
Power Management ICs
I am using a IR38063 to power my Intel Arria 10 Design... The initial design was based on the IR38063 Demo Board. I am seeing what seems like excessiv... Show More
Sakthivel
AURIX™
Hello there, Please share the difference between the parts "SAK-TC397XX-256F300S BD" and "SAK-TC397XX-256F300S BC" 1. we found the part "SAK-TC397XX-2... Show More
txgordo
Nor Flash
I am trying to clear (i.e., write to 0x00) the NVDLR register after having programmed it to a previous value.  I did see a post from 2019 that stated ... Show More
anil_sun
PSoC™ 5, 3 & 1
Hello,I'm trying to stream data with usbart in my project. Since I'm new, there were mistakes in some places that I couldn't understand.When I try to ... Show More
CoLy_3905441
PSoC™ 4
I am trying to enable the VBUS pin as an interrupt to wake my device.  It is self powered and goes to sleep as required, but I want to wake it up when... Show More
ritwik
USB superspeed peripherals
I am trying to use FX3 with OV7670 and following the instructions mentioned in AN75779 and on this Link Embedded Engineering : DIY USB 3.0 Camera: UVC Video Device Class VGA Camera Using Cypress FX3 (circuitvalley.com)... Show More
cmq_nj
IGBT
  如上图片,这是型号FF600R17ME4_B11的IGBT,有几个疑问:1,拆解实物看,里面有6个IGBT晶圆,6个2极管晶圆;规格书中拓扑图是2个IGBT和2个2极管符号,请问:结合实物图,是不是拓扑图中一个IGBT由3个晶圆组成? 2,规格书中的IGBT热阻 是不是一个IGBT中3个... Show More
jnagy
USB superspeed peripherals
I am streaming UAC audio from an FPGA to the USB host using the Windows Camera application and am experiencing backpressure I think is from the FX3 - ... Show More