Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Welcome to the Infineon Developer Community

  • 65218 Discussions

  • 37947 Members

  • 36648 Solutions

Recent discussions

Sort by:
Filter by forum
Tim_Shih
XMC™
Dear Receive, How to build a selected file in DAVE 4.5...?! I found there is a function that can be built a selected file but when I pressed it and no... Show More
happyeveryday
AURIX™
The TC397 does not have a TIF interface, can I use GPIO to emulate the TIF driver? For example, by using GPIO external interrupt to detect camera VSYN... Show More
happyeveryday
AURIX™

hello all,

Can the TC397 sample square waves with frequencies up to 50Mhz and How to configure if possible?

aneedles
iMOTION™ controller, driver & IPM
Hi, I am connecting up the iMotion-Link for the first time. I understand from my previous post (see link below) that I can use 5V logic on the target ... Show More
derkarower
USB EZ-PD™ Type-C
Hi, I'm facing a problem while developing the firmware for a 100W power adapter. I programmed the CYPD3196 via SWD and J-Link. Afterwards I could not ... Show More
CaelebMcKee
Gate Driver ICs
Hello there, I am attempting to run a Altium SPICE simulation with the SPICE model for the IRS21876S, and I'm encountering a few errors. I keep gettin... Show More
charlie
USB superspeed peripherals
Hello, Could you confirm if AT24CM02 256KB EEPROM can be used for FX3 I2C boot? Did Cypress do any testing with any 256K Atmel memories? Thanks you!  ... Show More
Shambhu
AURIX™
Hi, I am trying to generate the correctable alarm0[6] in SMU (for example: CPU0 SRAM PCACHE/PSPR single-bit correctable). but it was not generating, t... Show More
Bayou
AURIX™
I first tried to install : Infineon-Memtool-DevelopmentTools-v05_00-EN.exe on my windows 10 PC (this installer has been successfully installed else wh... Show More
rohit_ccrete
IGBT
I am currently using a setup with a FF1400R12IP4 IGBT with a corresponding 2SP0320TA0 gate driver. I have verified that the diodes are working in the ... Show More