Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Welcome to the Infineon Developer Community

  • 86053 Discussions

  • 103990 Members

  • 49914 Solutions

filter icon

Featured Discussions

Sort by:
Filter by forum
sujay_einfo
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
Hello, I am using imx8mn device & its running on android 9 2.3.4 OS. I want to connect my smartphone to the iMX8mn using Bluetooth. Once connection is... Show More
Pradeep_23
LED Driver ICs

Kindly advise, could we use XDPL8221 for Max output power upto 220w for Led Driver

YuTa_4942221
MOSFET (Si/SiC)
Thank you always.Let me confirm one point regarding 1200V discrete SiC. 【question】Is it possible to receive FBSOA for IMZA120R030M1H and IMZA120R040M1... Show More
etorlak
PSoC™ 5, 3 & 1
Hi fellows, Could anyone tell why I receive a run time error related to comparison of integers, something like this: uint64_t myNum; if(myNum >= (uint... Show More
DaAd_2521561
PSoC™ 6
I’m trying to add a USB Virtual Com port to my Free RTOS application using the emUSB library.   I added the mtb-example-psoc6-usb-cdc-echo example cod... Show More
HoiHo
XMC™
Hello everyone, I am changing the BCM5241 PHY to ADIN1200 PHY, because BCM5241 is obsolete. My source code works fine with the BCM5241, but there seem... Show More
user_4495571
PSoC™ 5, 3 & 1

Hi,

for my UART port pins there is no API generated.

Under Mapping Contiguous is selected.

Whats going on?

charles-weikeng
PSoC™ 4

客户产品量产阶段出现芯片不停复位,经过分析确认是看门狗复位,调整看门狗喂狗时间解决问题。能否提供温度对内部时钟影响的曲线图,谢谢!

chandru
AIROC™ Bluetooth
Hi, when Im using HFP handsree example code,  we are facing issues 1.In the handsfree_connection_event_handler function , we commented status  as I me... Show More
Clyasenth
Smart Power Switches
Hi, I am using TLE9104SH as a low-side switch. I want to control it with IN1,2,3,4, not from SPI. According to the datasheet, for enabling the output ... Show More