Welcome to the Infineon Developer Community

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question
  • 60604 Discussions

  • 34349 Members

  • 32075 Solved

Recent discussions

Sort by:
Filter by board
Go
awallace
PSoC™ 6
PSoC Creater 4.4 will program my CY8KIT-059.However, Programmer 4.00 will not recognize the device.However, Programmer will detect my CY8KIT-147.What ... Show More
Georges_Lab
MOTIX™ MCU
Dear Engineers, I'm using own application based on TLE9879 Eval Kit Hall Sensor example. Everything is working flawlessly but I'm unable to reach decl... Show More
ms360
ModusToolbox™ General
Hi! I am new to Modus and psoc6. I have a few questions about Release vs Debug builds. 1) The Makefile CONFIG variable seems to be the way to build th... Show More
wcc3
PSoC™ 6
The attached workspace bundle contains two projects:  a bootloader minimally modified from CE216767, Bootloader_DevKit, and a very simple bootloadable... Show More
StephenMc
PSoC™ Creator & Designer
I am using Creator 4.4 and I am trying to modify the API code for a existing component (TCPWM_P4_v2_10).I imported the component in my design and modi... Show More
MaFa_974161
Wi-Fi Combo
Hello. We develop a board with the same processor in CYW943907AEVAL1F. We mount CYPRESS S25FL064LABNFI010 instead of MX25L6433FZNI as FLASH.   I modif... Show More
aniruddhann
PSoC™ 6
Hi, while porting WHD, I have similar question as https://community.infineon.com/t5/Wi-Fi-Combo/Support-for-porting-WHD-to-stm32F7/m-p/212755 . 1. How... Show More
GergelySimon
USB superspeed peripherals
Hi there, We are seeing an issue with our design that is very similar to Solved: CYUSB3014 freezes during Slave FIFO transfer - Infineon Developer Community... Show More
TeMa_2997106
USB low-full-high speed peripherals
Earlier, I asked in the thread below if there was a Linux driver for VCP conversion.https://community.infineon.com/t5/USB-low-full-high-speed/CY7C65215A-VCP-support-for-Linux/m-p/327751#M10157... Show More
wowi
USB superspeed peripherals
We use the FX3 slave FIFO interface between USB and an FPGA device as described in AN65974  and observe that after ending the software it is not longe... Show More

2021 Community Wrap-up

Happy New Year! Let's take a look at the major achievements and memories from 2021 for our community.
Read more here.

Learn more about the Community

Review content or ask a question
Top liked authors